Title

Pokušajte pretraživati po ključnim riječima, kodu narudžbe ili proizvoda ili serijskom broju, npr. „CM442“ ili „tehničke informacije“
Unesite minimalno 2 znaka za pokretanje pretrage.

Condition monitoring at Gaasperdammertunnel in Amsterdam

How a digital solution helps to lower maintenance costs and supports predictive maintenance

11 lanes distributed between 5 tunnel tubes. 73 meters wide with capacities for up to 150,000 vehicles per day. Lush park landscape above over a three-kilometer stretch: The Gaasperdammertunnel in Amsterdam is one of the largest and perhaps most spectacular tunnel in the Netherlands. To ensure its smooth operation, IXAS, the operator of the tunnel, and the Dutch Infrastructure Authority Rijkswaterstaat are relying on SICK Belgium (now Endress+Hauser Netherlands) as a service partner.

Erwin Bes (Maintenance Engineer at IXAS) describes the benefits of the digital solution at Gaasperdammertunnel

Analyzers equipped with the condition monitoring feature from the Monitoring Box digital solution ©Endress+Hauser

Analyzers equipped with the condition monitoring feature from the Monitoring Box digital solution

The results

  • Thanks to the condition monitoring feature from the Monitoring Box, IXAS is always in the right place at the right time, and the concrete recommendations for action for the servicing personnel significantly reduces the maintenance costs for IXAS.

  • This project is transferable to any kind of tunnel. Operating companies who decide on this solution can benefit from numerous advantages, such as lower costs and fewer service deployments as well as improved maintenance scheduling.

  • The project in the Dutch metropolis was judged by all involved to have been a great success. Together they implemented a concept that meets the high expectations of the road users, the tunnel operating company as well as the authorities.

  • This article was first published on www.sick.com on October 18th, 2022. Since January 1st, 2025 Endress+Hauser exclusively markets SICK’s gas analysis and flow measurement technology worldwide.

Key visual success story condition monitoring in Gaasperdammertunnel Amsterdam

"IXAS has transformed from a reactive organization to a proactive one. With Monitoring Box, we are now far more forward-looking. It is much easier for us to plan and to adapt our plans as necessary."

Ing. E.W Erwin Bes, Maintenance Engineer
IXAS

The customer requirement: Clear view at all times

To ensure the highest level of safety in the tunnel pipes, in particular as the volume of traffic increases, accurate measurement of the visibility is essential. The VICOTEC450 visual range measuring device draws air out of the tunnel space, heats it up above the dew point, and determines the visibility using the laser light scattering method. The tunnel sensors continuously monitor the contamination and measure the air flow. Using condition monitoring, it is possible to detect ahead of time when cleaning or a filter change is required.

Our solution: Data transparency increases availability

To ensure the smooth operation of the tunnel, servicing and maintenance must be well structured. To optimize these and reduce faults to a minimum, IXAS decided to equip the analyzers with the condition monitoring feature from the Monitoring Box digital solution.

With condition monitoring providing a stable foundation on the path to predictive maintenance, maintenance work can be detected early, reduced, and optimized. It shows, for example, what work is required on which analyzer, and how it should be carried out. Maintenance tasks such as replacing filters are performed cost-effectively by IXAS. SICK Belgium (now Endress+Hauser Netherlands, see Portfolio and expertise strengthened) supports the operator as a reliable partner and takes care of the annual maintenance of the sensors. This collaboration brings several advantages to IXAS: Maintenance tasks can be planned in a more predictive manner and incidents resolved more quickly. Faults that would interrupt the tunnel operation are reduced to a minimum. Instead of assessing the systems on site in the tunnel, there is a constant flow of data that allows them to be monitored in real time. This makes IXAS faster, better prepared, and saves time and money on materials, spare parts and labor costs.

A further advantage for IXAS is the ability to not only integrate the data from the analyzers into the condition monitoring but also other devices from third party suppliers.

Monitoring Box Dashboard ©Endress+Hauser
Monitoring Box Dashboard ©Endress+Hauser

Tailored cybersecurity concept

To comply with the specific data security requirements of the tunnel, the local authority RWS Niederlande, the software development department, the cybersecurity and IT team at SICK, and the IT department of the customer have been working closely together.

The result is a cybersecurity concept that meets the most stringent standards: the smart service gateways are connected to the VICOTEC450 via a unidirectional data transfer and upload the acquired data into the cloud via a local Internet access in accordance with the industry standards for data transmission. To further protect the data transmission, the connection has been enhanced with a site-to-site VPN solution.

Kontaktirajte nas

Zanima vas naša ponuda? Željeli biste razgovarati o svojoj aplikaciji?

Javite nam što detaljnije o tome kako vam možemo pomoći

  • Jednostavni proizvodi

  • Jednostavno je odabrati, instalirati i rukovati

Tehnička izvrsnost

Jednostavnost

  • Standardni proizvodi

  • Pouzdano, robustno i s malo održavanja

Tehnička izvrsnost

Jednostavnost

  • Vrhunski proizvodi

  • Izuzetno funkcionalno i prikladno

Tehnička izvrsnost

Jednostavnost

  • Specijalizirani proizvodi

  • Dizajnirano za zahtjevne aplikacije

Tehnička izvrsnost

Jednostavnost

Promjenjivo

FLEX odabir Tehnička izvrsnost Jednostavnost
  • F
  • L
  • E
  • X

Fundamental odabir

Udovoljite svojim osnovnim potrebama u mjernju

Tehnička izvrsnost
Jednostavnost
  • F
  • L
  • E
  • X

Lean odabir

Jednostavno upravljajte svojim osnovnim procesima

Tehnička izvrsnost
Jednostavnost
  • F
  • L
  • E
  • X

Extended odabir

Optimizirajte svoje procese s inovativnim tehnologijama

Tehnička izvrsnost
Jednostavnost
  • F
  • L
  • E
  • X

Xpert odabir

Ovladajte svojim najizazovnijim aplikacijama

Tehnička izvrsnost
Jednostavnost

Promjenjivo