Title

Pokušajte pretraživati po ključnim riječima, kodu narudžbe ili proizvoda ili serijskom broju, npr. „CM442“ ili „tehničke informacije“
Unesite minimalno 2 znaka za pokretanje pretrage.

Industrial asset management as the foundation for scalable maintenance optimization

Building a secure foundation to improve asset performance and effective maintenance at scale.

Industrial asset management: Man standing in front of a plant with an tablet

Equipment maintenance strategies define how maintenance is carried out, including the methods, intervals, and technologies used to keep a process plant running. Industrial asset management determined how maintenance decisions are made across the installed base. It provides the context needed to decide where a strategy should be applied, when intervention is justified, and which assets are critical to the process.

In process industries with aging instrumentation, mixed lifecycles, and growing regulatory pressure, industrial asset management becomes the critical decision‑making layer between maintenance strategy and execution. Additionally, it creates the foundation for asset performance management, enabling organizations to manage asset health, risk, and performance consistently across the entire installed base to ensure the plant is running at peak performance.

Industrial asset management in the maintenance journey

Industrial asset management makes asset condition, lifecycle status, and criticality visible across the installed base. Its purpose is not execution, but transparency, consistent decision‑making, and determining where maintenance effort matters most.

By establishing a shared, asset‑level decision framework, industrial asset management defines what should happen next. Prioritized decisions must be executed reliably through structured work order management. Over time, their outcomes must be evaluated and improved, enabling maintenance optimization at scale.

In this way, industrial asset management forms the link between insight, execution, and optimization, ensuring maintenance actions are driven by asset reality, not fixed routines.

Connecting maintenance strategies with asset‑driven performance decisions

Maintenance strategies answer the question of how maintenance should be performed. Industrial asset management answers the questions of how decisions are made across the entire installed base, rather than just one work order, or one asset at a time.

By creating a structured view of the installed base, industrial asset management provides the visibility and context needed to apply maintenance strategies consistently and effectively. It forms the bridge between strategy, execution, and ongoing optimization, ensuring that effort is focused where it reduces operational risk rather than following fixed pre-determined intervals.

What industrial asset management means in process industries today

In process industries, industrial asset management is best understood as a decision framework for the installed base. It supports maintenance and operational teams working in environments characterized by long asset lifetimes, mixed generations of instrumentation, and strict safety and compliance requirements.

Rather than focusing on individual maintenance actions, it applies asset data to govern consistent, risk‑based decisions across the installed base.

A central element of industrial asset management is transparency. It establishes a single, trusted view of what is installed, where it is located, how it is configured, and what condition it is in.

Managing asset lifecycle status and obsolescence to protect asset performance

Asset performance is influenced not only by condition, but also by lifecycle status. As instrumentation moves through the lifecycle, risk inherently increases gradually even if equipment continues to operate.

Industrial asset management makes lifecycle and obsolescence status visible and actionable. It enables organizations to understand which assets remain fully supported and which introduce increasing operational or safety risk.

This lifecycle insight supports structured decisions on replacement and risk mitigation. By proactively managing lifecycle risk, industrial asset management protects asset performance and prevents unplanned inefficiencies caused by unsupported or obsolete assets.

How industrial asset management complements maintenance execution

Industrial asset management and maintenance management are complementary but serve distinct roles.

Maintenance management focuses on planning, scheduling, and executing work. Industrial asset management provides the asset‑level context and prioritization that guide those activities, forming the frame and helps to outline a strategy. It ensures that maintenance effort is applied consistently and based on risk, rather than solely on pre-defined intervals, such as time or once a process threshold has been reached.

At the same time, industrial asset management goes a step further and enables asset performance management by providing reliable asset data, lifecycle transparency, and decision logic. Rather than replacing existing strategies or systems, it strengthens them by aligning execution and performance goals across the installed base.

Optimizing asset health, performance, and risk across aging and mixed installed bases

Most industrial plants operate a mixed installed base with instruments, systems, and software at different lifecycle stages. Assets differ in criticality, failure modes, and operational impact, which makes uniform maintenance approaches inefficient.

Industrial asset management enables both risk‑based prioritization across this complexity and the optimization of maintenance strategies across your installed base. By making asset data visible, it supports asset performance management efforts aimed at improving availability while controlling cost and effort.

This approach allows teams to reduce over‑maintenance, focus resources where they deliver the greatest value, and maintain control as assets approach failure, or obsolescence.

How industrial asset management turns decisions into results

Once asset data is consolidated and contextualized, industrial asset management turns insight into action. It connects understanding with both execution and optimization, helping teams move from visibility toward measurable impact.

By defining priorities at the asset level, industrial asset management naturally leads to structured execution through work order management and continuous improvement through maintenance optimization.

Automated work order management: A man and women looking at a tablet in an office setting

Decision to execution - Digital work order management

Once you have prioritized assets and actions, those decisions must be executed consistently and efficiently. Digital work order management ensures asset‑driven priorities are translated into clear, traceable maintenance tasks, without manual coordination or interpretation. This connection is essential for effective asset performance management, as it ensures execution aligns with asset driven priorities rather than reactive events. Find out how to execute prioritized asset decisions.

Digital maintenance optimization: Man looking at a tablet in front of a wall of devices

Execution to optimization - Scaling maintenance optimization

When asset‑driven decisions are executed consistently, their outcomes become measurable. This creates the basis for maintenance optimization, allowing organizations to balance cost, effort, and risk across the installed base instead of optimizing individual assets in isolation. Industrial asset management turns device data into insights operators can use to optimize maintenance activities. Discover how consistent execution enables maintenance optimization at scale.

Measuring success in industrial asset management and asset performance management

Industrial asset management does not replace operational KPIs, but it helps organizations govern them more effectively and efficiently. By providing consistent asset context, it supports performance measurement across several dimensions, including:

  • Planned vs. reactive maintenance ratios
  • Asset availability trends
  • Lifecycle and obsolescence risk exposure

Together, these indicators help maintenance and plant management assess whether decisions are reducing risk and improving performance across the installed base.

Industrial asset management is effective only when its decisions are applied consistently and improved over time. Structured execution and maintenance optimization ensure that asset‑driven priorities translate into measurable performance across the installed base.

Frequently Asked Questions

Završne napomene

How can we support you on your digitalization journey?