Pokušajte pretraživati po ključnim riječima, kodu narudžbe ili proizvoda ili serijskom broju, npr. „CM442“ ili „tehničke informacije“
Unesite minimalno 2 znaka za pokretanje pretrage.

Calibration services at Milchwerke Schwaben

Reliable service from Endress+Hauser leads to satisfied customers

Endress+Hauser has been managing Milchwerk Schwaben from the service side for many years, whether it involves rectifying a malfunction, commissioning new measurement instrumentation, carrying out maintenance on the installed base of process control technology or inspecting and calibrating the measurement instrumentation. Milchwerke Schwaben is committed to financial, ecological and social responsibility.

Calibration on-site of a pressure instrument ©Milchwerke Schwaben

On-site calibration of a pressure instrument

Calibration documentation ©Milchwerke Schwaben

Calibration services with clear and comprehensive documentation

Our solution

  • At Milchwerke Schwaben, 15 percent of the total energy needs is covered with steam. To ensure accuracy, the relevant instrumentation (pressure, temperature, flow and energy monitoring) is regular inspects and calibrated.

  • Endress+Hauser developed an individual calibration strategy that included a time-saving concept. The multistage inspection concept makes removal of the instruments only partially required.

Weideglück Logo

“We rely on the expertise of Endress+Hauser. And the best thing is, this leaves us more time to focus on our own core expertise: producing regional, high-quality dairy products.”

Meinhard Schuler, Head of production
Milchwerke Schwaben eG, Germany

Challenge

In order to be able to continuously supply its domestic and international customers with superior quality products in line with up-to-date science and the latest regulations, Milchwerke Schwaben is IFS-certified (International Food Standard). The company also observes the highest standards when selecting its raw materials and operational supplies. Start-to-finish controls, from raw material processing on to delivery, are a guarantee for the high quality of the company’s milk products.

State-of-the-art measurement technology

Milchwerke Schwaben uses the latest technology, which allows the verification to be carried out with the Heartbeat technology without having to remove the instrument and interrupt the process. In addition, regular investments are made in the latest measuring technology in order to be able to produce regional products as efficiently as possible and to meet the high quality standards.